Posted on May 17, 2011 at 09:53Yes lillian_200601! That's exactly what I had to change... and not more crash. One would think that if the GPIO_IPConnected parameter was incorrect, it would simply cause the UART to not work. Thanks for your input.
Posted on May 17, 2011 at 09:53I'm using the MCB-STR9 development board and wanted to initialize Port6.7 to utilize UART0 Tx. The documentation says this is possible by way of Alternate Output 3 for Port6 Pin7. After calling GPIO_Init() the chip see...
Posted on May 17, 2011 at 09:50Hi, correct me if I'm wrong, but after looking at that posted code, I notice that the rising/falling edge bit is actually set for interrupt 6, not 5. Could this be causing some of your issues? Posted: 4- WIU set up WIU...
Posted on May 17, 2011 at 09:33Hi, I ran into this same problem... RAJ, could you please post the solution? Thanks in advance, Dave [ This message was edited by: dbarbarine on 25-02-2008 19:31 ]