Posted on May 17, 2011 at 13:05Well that evaluation board had a seperate xtal for the Phy. This means it did not answer the question. I would suggest driving the stm32 and the phy from the same oscillator module. We have an ARM based project (not st...
Posted on May 17, 2011 at 12:56I read this thread when it was written and was interested in any updates on new products from ST. I see nothing happened. I have seen early information about the STM32L and would like to use chips such as I saw in a ne...
Posted on May 17, 2011 at 12:24I have used c++ in an embedded environment on ARMs for years. It has been on ones with external SDRAM. I considered using C++ on a small application for the NXP LPC2103. I did not in the end just for the sort of reason...
Posted on May 17, 2011 at 12:22I have had a go at getting the SD Mass Storage Demo working on the Keil Board. I leave some notes here to help people trying this in the future. Firstly the chip is different between the two boards. They are both 103's...
Posted on May 17, 2011 at 12:22I have downloaded this demo. I have 2 questions. 1) What modifications would be required to make it run on the KEIL MCBSTM32 board. 2) Is MMC cards supported. Thanks.