Hello, we don't have a dedicated solution for 240W yet. Our solution can handle up to 60W at the moment. Please check our STPD01 DCDC converter which has USB-PD dedicated functions which simplify the USB-PD development.https://www.st.com/en/power-man...
HI AndrewIt's not clear to me how you would like to use the LGATE. The freewheel diode (or FET) is in high side in a Boost topology, so it cannot be driven by LGATE. This is the reason why we suggest to implement asynchronous Boost with L6726. In an...
Hello Andrewyou can use the L6726 to impement an Asynchronous boost converter. Use the UGATE pin to drive the main switch of the boost. PHASE pin has to be connected to the source of the switch (i.e. to GND). The booststrap cap has to be connected b...
HelloThe STNS01 is designed to have a very low quiescent current during the operation in Battery mode, so the LDO, being a low quiescent current, has a slow dynamic response versus line(input variation) variation. This creates the problem you are fac...
HelloI'm not sure if I well understood your question. However, please check the STPD01 DCDC converter. It provides power with easy to use I2C interface to select the right PD profile. However, its maximum input voltage is 26.4V, while I understand yo...