Posted on May 17, 2011 at 12:48Thanks guys, My plan is indeed to use one master that polls the slaves and to use the 9bit mode similar to 8051 (all in mute). The slave will speak only if spoken to. I'm also planning to ultimately use RS485 different...
Posted on May 17, 2011 at 12:48Hi, I need to connect 6 or 7 STM32 together, with one STM32 used as a master and the other one as slaves. The flow could be half duplex or full duplex. I could use the I2C interface but I'm tempted by the intrinsic sim...
Posted on May 17, 2011 at 12:48Hi pandoraems, Did you set the BDU bit to '1' inside CTRL_REG2? This will make sure no temporal discontinuity will occur. Regards