Posted on May 17, 2011 at 12:38As stated in user manual multimaster mode is not supported if NSS output is enabled. I really don't understand what is the purpose of NSS hardware mode. If one device is configured as master and other as slave why woul...
Posted on May 17, 2011 at 12:38I put 6.8k pull-up to NSS line. Until SPI_Cmd(SPI2, ENABLE); NSS stays high, then it goes low and stays there. But if I add SPI_Cmd(SPI2, DISABLE); after the transaction it will go up again.I confirm that this is how R...