Posted on May 17, 2011 at 12:23I want to download the hex or axf file thr' JTAG port. I am using KEIL uvision tool with ULINK2 programmer. But i don't have the code compiling in the scope. i want to download hex file. Please let me know the tool set...
Posted on May 17, 2011 at 12:22I am new to STM32F101 family. what tool can i use for programming this device? Which tool provides the JTAG interface to the ULINK programmer?
Posted on May 17, 2011 at 12:19I am using STM32F101 device.It is 3.3V operating. I want to interface 5V compatible LCD to microcontroller. Are the I/O pins of microcontroller are 5V TTL compatible?