2008-02-08 06:15 AM
FLASH loading thr' the JTAG port
2011-05-17 03:23 AM
I want to download the hex or axf file thr' JTAG port.
I am using KEIL uvision tool with ULINK2 programmer. But i don't have the code compiling in the scope. i want to download hex file. Please let me know the tool settings & steps for download2011-05-17 03:23 AM
Hi,
You can use plenty of tools thru JTAG or SWD : you can refer to our web page :http://www.st.com/mcu/contentid-102.html
even better you can simply use the USART ( RS232) and the internal bootloader if you do not need JTAG as well 🙂 Regards, STOne-32