Posted on May 17, 2011 at 09:49Hi, Have anyone evaluated STR9 comstick's ADC.The digital o/p is 03ff when my analog input is only 2V.On the datasheet. it states the range is between 0 and 3.6. It seems like the ref voltage is at 2 but the schematic ...
Posted on May 17, 2011 at 09:49Hello, For Adc configuration, do i need to configure the ip connected enable in the gpio setting? and what is that for? Thanx! Regards, Gan Zhiheng
Posted on May 17, 2011 at 09:49Hi , i am using a winsock application to send a short data like ''cc'' to the uip web server. But i cannot find the data in the buffer. it only acknowlege the connection. Could i know what may be the problem? Thanks la...
Posted on May 17, 2011 at 09:49Hi Mjbc, Thanx for ur help!! So i get the data from the address in the buffer descriptor rite ? Thanx alot Regards lazycat