Posted on May 17, 2011 at 12:18Hi again, I solved the problem. The solution is to enable Hardware NSS Pin Management. You then have two options. BTW, this probably only works in Slave Mode. 1: Configure the NSS PIN in GPIO Mode ''AF_PP'' like in the...
Posted on May 17, 2011 at 12:18Hi, I've been programming with the STM32 for a few weeks now. Right now I have a task which I was hoping to solve with the STM32's SPI. The Task is to Output 25bit Data on an external clock. I configured the SPI1 in sl...