Posted on May 17, 2011 at 09:53tnk, I have resolved the problem trought the function of WIU and VIC library. Port 6.0 ---->interrupt16 (see manual and the Wic' example) Port 6.4 ---->interrupt20 Using thus functions ( taken advantage from the struct...
Posted on May 17, 2011 at 09:53Hi, I have to controll the port 6, pins 0 and 4, that rappresent two signal from an encoder. I try first to envelope the SW for the first port with interrupt. The problem is that don't run. Can you help me, please? thi...