Posted on May 17, 2011 at 12:57hello friends i am using stm32f103, Is there any core register which can provide the cause of last reset? I cannot use debug as there is no jtag port on my board I got a situation where mcu reset randomly and this occu...
Posted on May 17, 2011 at 12:55Due to design limitation I have to use one of the jtag interface pin(JTCK) as input, but i cannot configure it as any other normal pin, not even as output. According to datasheet it is input pull down at reset, but how...
Posted on May 17, 2011 at 12:30i am working with I2c eprom 24c16 type, at first i am using example5 of ST 's i2c examples. But what happening is i cannot able to write on two consecutive steps using I2C_EE_BufferWrite function. it hangs after writin...
Posted on May 17, 2011 at 11:32When i download latest data sheets of Str 9 family it has water mark of obsolete product. So is str product line is obsolete now? please reply.