ariel
Associate
since
2018-07-19
2023-06-14
User statistics
2
Posts
0
Solutions
0
Kudos given
0
Kudos received
STMicroelectronics Community
About ariel
Options
Report User
User Activity
Posts
Replies
STR751FR0 with a single supply of 5 Volts
2008-06-04
Posted on June 04, 2008 at 14:41STR751FR0 with a single supply of 5 Volts
Re: STR751FR0 with a single supply of 5 Volts
2008-05-19
Posted on May 19, 2008 at 10:54 In the power schemes in the STR751FR0 data sheet it is written that there are four power schemes ,single 3.3V or 3.3V + 1.8 V or single 5 V or 5V+1.8V. But in the table of the same data sheet HEREBY ATTAC...