Posted on September 26, 2007 at 07:00Dear SCo, thanks for answer. The ''Debug Instrument Selection:'' is ''lcd Rlink'' and the ''Target Port Selection:'' is ''usb://usb''. Programming the ''...s19'' file into the hardware works fine with the Rlink u...
Posted on September 25, 2007 at 07:10Has nobody experience with ''Rlink'' as debugger together with ''ST7VD'' ? Why does the programming work with the ''Rlink'', and the debugging gives the error message ? Nobody an idea ? Have a nice day, Hilde
Posted on September 24, 2007 at 11:10Dear community, I have an application for the microcontroller ''ST7FMC2S4'', compile my program with ''Cosmic'' compiler and then program the object code either with the ''STICK'' programmer or with ''Rlink'' int...