Posted on March 03, 2008 at 12:49Hi all, I have programmed an IAP application in order to load other programs remotely. I am using ARM7 STR7. Now I got two microcontrollers ''blocked'', when I try to reprogram these I always get the following messag...
Posted on October 02, 2007 at 11:51I am refer to the first decision. If the P0.15 is active then launches the Remote Loader application else jumps to the user program.
Posted on October 01, 2007 at 13:37 I am using the port as input as a condition to jump or not, in the image attached you can see what I mean. Then, the problem is that if I use the port 1.2 the download is done correctly and the execution as...
Posted on September 27, 2007 at 14:26Hello, I was using the I/O port 0.15 in the STR710 FZ2 as a selector to program a Remote Loader. Using this pin the program were being stored correctly but the execution failed. I changed to the I/O port 1.2 and ...