Posted on May 17, 2011 at 13:08There is also a problem when using a COM port higher than 9. At least with W2K SP4. We are using an USB-serial converter. When changing the port number to <=9 everything works except for the optimize bug.
Posted on May 17, 2011 at 13:08Loader Demonstrator 1.3 does not write correctly to the target if ''Optimize'' is checked. If the attached file is programmed using ''Optimize(remove some FF)'' address 0x0800AFFF will be 0x20 instead of 0xFF as it sho...
Posted on May 17, 2011 at 12:36I reply to my own message. Flash Loader Demo 1.1.1 seems not to be able to handle COM ports bigger than COM9. My USB to serial adapter was initially on COM11 and did not work with Flash Loader Demo 1.1.1. After changin...
Posted on May 17, 2011 at 12:36Hi, I have downloaded and installed the latest 1.1.1 version. I try to connect to the target using an USB-RS232 converter from FTDI called TTl-232R-3V3. This is COM11 on the computer. Using hyperterminal I am able to s...