Posted on October 08, 2007 at 06:55Hi, I wonder if anyone could help me on RTC of ST10F276. I want RTC to use low power 32kHz oscillator. The OSC bit (oscillator selection flag) in RTCCON register is read only. Can oscillator clock of RTC be selecte...
Posted on September 11, 2007 at 09:09 Hi Najoua, Please find attached code witch used to transmit/receive data from/to XBUS serial interface. I use Advanced Serial Port Monitor to send and receive data from processor. Thank you very much...
Posted on September 06, 2007 at 15:25Anyone can help me on following two problems regarding XASC & ASC0 of ST10F276. The two serial interfaces are configured to be RS485. We use P8.4 toggling between transmitting and receiving for XASC; use P8.3 tog...