Posted on August 27, 2007 at 11:21Hi everybody ! I use the ADS IDE (with Metrowerks Codewarrior for ARM) to work on the STR7, and I have some difficulties to configurate properly the project files, and make the example projects work. The ST archives...
Posted on August 09, 2007 at 08:18Another question : when I enable the interruptions, instead of staying around the while loop I am not been able to go out, sometimes the program seems to ''crash''. When I stop it during debug, I am into a list of d...
Posted on August 06, 2007 at 07:49sjo > OK now I see I'm using Metrowerks CodeWarrior, so I don't use gcc as a compilator... The variable is declared with the u16 type only. ben_fnr > When I connect the card to the computer, my PC tells me it sees...