Posted on July 25, 2007 at 06:13Hello I modify the str711 Mass Storage demo,when I want to read from the USB device,the fisrt time it read 16 bytes what are not my want,then the sencond and third time ,it is right. But when I power on again,it repea...
Posted on July 24, 2007 at 23:15Thank you for you help Do you mean that I must set In point in valid status before the host send a IN packet to str711 board? Should I set IN point in valid status in MASS_Reset()?
Posted on July 24, 2007 at 13:55Hello, I use ST Mass Storage demo(Simple Buffer) and DDK�DriverStudio to generate a host application ,but I find that when I want to read from the ST board,it does not enter the CTR_LP() How can I solve the problem?
Posted on July 22, 2007 at 23:37Hello I'm using STR711 I'm trying to use USB Mass Storage Device program of the USB dev Kit (UM0290) to transfer something,but I have some troubles When the USB cable is plugged in Windows does not recognize the devic...