Posted on May 17, 2011 at 12:19Quote: You mean table 48? Analog power supply equal to VDD and 2.4 V ≤ VDDA ≤ VDD (3.6 V) The first line says they must be equal, the second that VDDA must be above 2.4V Hi obtronix, Conveniently missed that firs...
Posted on May 17, 2011 at 12:19Quote: no the part will be destoyed if |VDDA-VDD| >.05 volts, see table 4Hi obtronix, Are you sure that VDDA cannot be different from VDD, I had a look at the datasheet and can see that |�?VDDx| In the STM32 Reference...
Posted on May 17, 2011 at 09:45Thank you very much, Will have a look at that. I will also have to create the fat in code, as I need to write data to a file. So I will start with that part Regards, Gert
Posted on May 17, 2011 at 09:45Hi, I would like to send some data(quite a lot actually) to the pc. It looks like the best way would be to use the USB bulk transfer demo, and work from there? I have the data stored on an SD card (no fat file system a...