Posted on May 17, 2011 at 12:26Quote:On 01-04-2008 at 08:28, Anonymous wrote: ULINK2 offers all the features of the original ULINK USB-JTAG Adapter plus 10MHz JTAG clock, RTCK support, Serial Wire Debug (SWD) support, Serial Wire Viewer (Trace) supp...
Posted on May 17, 2011 at 12:26Quote:On 31-03-2008 at 09:45, Anonymous wrote: Hi It came out, that it could be used anyway, but if it is used with the STM3210B-MCKIT, you cannot use the optical print, if you want to debug. Then you have to connect ...
Posted on May 17, 2011 at 12:26Quote:On 25-03-2008 at 09:19, Anonymous wrote: ST has told me that the Ulink-me can not be used for the STM3210B-EVAL kit. Then you know it Please can you tell me if Ulink-me is for a specific evaluation board. Or w...
Posted on October 29, 2008 at 23:04Quote:On 29-10-2008 at 23:33, Anonymous wrote: Under the flash menu of your IDE you should find the erase command Thanks, i found it before but I wanted to delete without run the core. i solve this problem desolde...
Posted on October 24, 2008 at 01:01This is the bad of STR7. Lot of people do not want to share his knowledge and ST do not have a good suport. If I go to LPC forums, i get at least 5 answers. I say this not just for me. Many topics with 0 answers....