Posted on June 04, 2007 at 06:05Hello, can some body tell me wich hardware tool for debug and programm, can work with ST7LITE US5?. I have a Raisonaice RLINK but it doesnt work, I'm trayng to work with Rlink for more than 3 weeks, but not, also I ha...
Posted on May 29, 2007 at 05:52Yes all the jumpers are correct J4 an J5 are open and S2 is open also (button position). I externaly power the steval with 5 Vdc directly to condenser C5 and we check +5Vdc in pin 1 (refer to of F7 Ultralite (I do it...
Posted on May 18, 2007 at 08:12Hello, we are using a evaluation board : Steval-ILL004V2, is a phase control dimer. The CPU is ST7LITEUS5. I�cant communicate with Rlink, all the signals are correct : Reset, Vss, ICCCLK, ICCDATA, CLKIN, VDD and the ...