Posted on January 16, 2007 at 07:11Hi again, there are ''dead'' cycles when using the ART as INT source. To check this out, i programmed a simple software RTC using the ART OverflowINT as Timebase. Every INT increments a register til 40d. 25ms*40=1s...
Posted on January 05, 2007 at 06:41Hello Folks, i programmed the ART as freerunning Timer. Fosc= 3,6864 MHz, ClkDiv= 3, Prescl= 128 Fin= 9600, RC= 10h If my Calculations are correct, the above Settings = 25ms. The Overflow Interrupt is used to updat...