Posted on May 17, 2011 at 09:58I have a I2C interface driver that 99.9% of the time works OK but occationally fails for the same reason. After I issue the start bit and wait for the events of EVF, BUSY, SB and MSL to become TRUE, the BUSY sometimes ...
Posted on May 17, 2011 at 09:45Hi all, STR912F device I'm trying to get the ENET transmitter to work with more than one descriptor. Have got two descriptors linked together in a ring and I'm setting the NXT_EN bit within the ENET_TXCR register for b...
Posted on May 17, 2011 at 09:33Hi, Spent a week on this issue and I think I have a workable workaround that does work. Tried all the idea's mentioned here but alas they don't work, so here's mine which has been working for more than 24 hours errors ...