Posted on May 17, 2011 at 09:35Hi Vincent! Thanks for your advice I did what you said. I have correct version of IDE(746) and the example of AD converter runs all right. But I tried to insert a code for the interrupt of Timer1 into this example. B...
Posted on May 17, 2011 at 09:35Hi MBS! Thanks for you reply, but it is not what I need. I am able to translate the program and load to the Flash memory. The problem isn't in program code. But I don't know how to make available the interrupt routine ...
Posted on May 17, 2011 at 09:35Hi! I have a problem with StartUp in RIDE IDE. I use the STR912F processor and I have two development environments - KEIL uVision and Raisonance RIDE IDE. If I make the project in Keil, I must use the StartUp file str9...