Posted on January 17, 2007 at 10:21Hello, I'm using the STOP Mode as the Power Down mode for my hand held device. I'm using STR711FR2T6 controller for my application. As per the referance manual I should be able to wakeup my device by XTI pins[Risi...
Posted on January 10, 2007 at 23:49Hi Moderator, The Problem was with the Standby mode. If I use the LPWFI mode then the problem has been solved. Now the power consumption is 1.5mA. But I have to reduce the consumption to 100-200uA. I have put the ...
Posted on January 10, 2007 at 03:43Hi all, I'm using the STR711FR2T6 Microcontroller for my Hand Held Device. As it is a hand held device power consumption matters a lot. I have to put the Oscillator in the standby mode [in the Sleep Mode] so that ...
Posted on January 10, 2007 at 00:24Hi all, I'm using the STR711FR2T6 Microcontroller for my Hand Held Device. As it is a hand held device power consumption matters a lot. I have to put the Oscillator in the standby mode [in the Sleep Mode] so that ...