Posted on October 02, 2007 at 05:04Hello ! Thank you for the idea but the bug was still there. So I don´t know what can I do to save my hitex board without soldering the IC! Has nobody another concept to save my board? Best regards macke_a
Posted on September 27, 2007 at 04:33Hello everybody ! Has nobody an idea so what can I do to repair my controller without soldering the STR710 ? Best regards macke_a
Posted on September 21, 2007 at 11:28Hi ! I have check the hardware between the programmer connector and µC. There is everything fine. The Ulink is also ok. I have a second board with the STR710 controller to the checking my environment! Im sure th...
Posted on September 21, 2007 at 10:11Hello Coucou, thank you for answer! I have already check the idea to change the boot mode on the hitex evalboard. But nothing happend, the problem exits further! I have no access to my controller. The Keil presen...
Posted on September 20, 2007 at 13:58Hello! Since yesterday I am not able to programm my ''STR710FZ2 - Controller''! I use the ''Hitex STR7 Evalboard'' so that the hardware is all right built on. The ''JTAG Connection'' shows with the Keil µVison3 ...