Posted on May 17, 2011 at 09:44Hello, again helpless I have to note I have special CPU version STR912FAZ44H (so maybe it is my small local problem). So my target is to configure I2C interface in slave mode to receive command from master device and...
Posted on May 17, 2011 at 09:44Ok, so hopefully now my question is displayed in this forum.. Did anyone utilized external DMA request (DMA_RQST0 or DMA_RQST1 pin) to read or write data on EMI interface using DMA channel? The problem is, that I fou...
Posted on May 17, 2011 at 09:44Ok, I got response from ST support centre Resolving the problem with EMI_BCLK signal is simple. My configuration code as you can see in my previous post has been OK. But minimally one read or write access to EMI inte...
Posted on May 17, 2011 at 09:44Hello , I have CPU version STR912FAZ42, which is packaged in LFBGA144 and so it has connected pin EMI_BCLK on output pin M8. And now the question: Did anyone bring EMI_BCLK signal into run? I configured EMI into 8-bit ...