Posted on May 17, 2011 at 09:32Hi Stevejamal, The problem has been solved.The reason is the PIN P57/SSP0_NSS is connected to VCC via a Resistor( R118 10K in STR912-SK EVAL Board ). If this pin tired to VCC directly, it works, otherwise you will see ...
Posted on May 17, 2011 at 09:32Hi, I use IAR start kits STR912-SK to test the SSP-debug in the examples.eww workspace which is in ...\ARM\examples\ST\STR91x\STR91xlibrary\examples\directory. I made a cable to connect the SPI0 connector( Master )and ...
Posted on May 17, 2011 at 09:30Hi I have downloaded the FreeRTOS and choosed THUMB as configuration, then I rebuild the project, I got a message:Too much object produced( more than 0x8000 )for this package. The reason is I use the 32K limited compil...