Posted on May 17, 2011 at 10:13Hello, I'm preparing to develop BLDC motor controller board with ST7FMC. Before doing it, I plan to test it with st7fmc evaluation board. But STM have 2 kinds of st7fmc evaluation boards. They are STEVAL-IHM001V1 and S...
Posted on April 06, 2007 at 00:12Which tools do support STR750 or STR755 peripherals when debugging?. When I tested it on KEIL MDK-ARM 3.05, the peripherals of simulation debugging is good(but support just GPIO, UART, CLOCK, so on), But the peripher...
Posted on August 28, 2006 at 09:18Attached is the simple timer example by ST. I compiled it in EWARM and debugeg in C-Spy with J-Link. When I run it in my STR710-EVAL board, it run without a problem and REDs in the board blink in sequence. But, when...