Posted on June 06, 2006 at 05:45Hi, I tried this solution, but this will not work with a software reset. It works fine though with a hardware reset. To do this, an extra GPIO pin must be used for the reset pin to go low. I found another solution usi...
Posted on June 01, 2006 at 11:22Hi, I have tested a solution using a GPIO pin to set the level of M1 and then execute a software reset. It does noet work??? As soon as the software reset is executed the GPIO pin is input and the high level is not ma...
Posted on May 15, 2006 at 09:43I want to create a user friendly method in my application to enter SystemMemory Boot Mode without using reset and M1 pin. Is this possible or is a reset with M1 pin high the only method? If this is possible, my custome...