Posted on May 17, 2011 at 09:34hi,acorchia thank you for the help. the problem is, first I use flashlink to set bank1 as bootbank and write bank1 with program 1,it work normal. then I use flashlink to set bank0 as bootbank and write bank0 with p...
Posted on May 17, 2011 at 09:34Hello: the bootflash config bit is the 0x520006 BIT0 CSX,isn't it? Can i config this bit in my application program? if it be set ,does bank1 flash must map 0x0~0x7fff? if it be reset does the bank0 flash must map 0x0~...
Posted on May 17, 2011 at 09:31hi,STARM and acorchia: ''The CPU crashes because the FMI_Config function writes in the configuration registers of the flash which are located in Bank1.'' As i know the configuration registers of the flash is in 0x54000...