Posted on May 17, 2011 at 09:34Hi, the solution is to assign the both DVAR registers to a dummy IRQ hanlers. In case of not using the library IRQ handler (so jumping directly to the ISRs), the VARs should be also written to 0 at the end of the dummy...
Posted on May 17, 2011 at 09:33Hi, the solution is to assign the both DVAR registers to a dummy IRQ hanlers. In case of not using the library IRQ handler (so jumping directly to the ISRs), the VARs should be also written to 0 at the end of the dummy...