Posted on May 17, 2011 at 11:50Thank you for your reply. I have come up with the following, which I will be testing soon to see if it works. (I need to set up a test download w/o the full application in order to test). If there is anything in this i...
Posted on May 17, 2011 at 11:50I'll work on that. As I didn't write the original it may take a while to figure out where all of the configuration is being done. I had been hoping to just see how the configuration registers needed to be set to enable...
Posted on May 17, 2011 at 11:50I am attempting to add support for the second uart to an existing program ported from an 8051. I have had no luck getting any output from the second uart. I have Googled furiously and can find no example code for this ...