Posted on April 11, 2006 at 08:45Hi All, I tried this version:2 driver, but it never works for me. The program is started, but the downloading doesn't work. At the flashing point always stoped. If I debugging the program and step-by-step execution i...
Posted on February 16, 2006 at 11:26:p Thanks STARM!!!!!!! :p The unused clocks was OK. That's great! The PCU->PLL2CR|=0x0007; // stop the PLL2 missed. Now the Stop mode current is ~100uA. Thanks! Rachny :-] ;)
Posted on February 16, 2006 at 09:07Thanks STARM! :) The setting was succesful, but the current consumption of the STR712 is about 1mA. I don't use RTC clock, the external clock is disabled by a external hardware during stop mode. The wake-up is wor...
Posted on February 15, 2006 at 12:21Hi! My question is: how to enter STOP-mode with low current (by datasheet 100uA)? Which internal clocks and peripherial block have to disable to reach this minimum current? In the hardware I use CAN-module and the...