Posted on March 21, 2006 at 07:06Hi, Are they more than 32 bytes which are corrupted ? Sometimes YES and sometimes NO Our sector 0 size is 0.5 K Thanks B.PICARD
Posted on March 21, 2006 at 04:14I suppose that we are alone with our problem because nobody seems to get the same problem. But, Is there ST72264 users on this forum ? Thanks B.PICARD
Posted on March 14, 2006 at 05:46Hi, - when you check the failed content, is there several addresses ? YES (E001, E002, E003, E004, ... and sometimes up to the beginning of the code so the ST7 cannot run! is(are) the same address(es) from one part t...
Posted on March 10, 2006 at 06:26YES, we have implemented IAP routines in our application. BUT, we never launch an IAP session when it is running. We use IAP only at boot process and only if the revision of the ST7 is bad. When we program the ST7 wi...