Posted on May 31, 2006 at 09:13hi, i hope to have an unswer. I'm going explaine now the program: i'm using GPS data via SCI bus, en then each 10 second we should store data GPS in I²C memory. the problem is when 10s is reached, i can't write to I²...
Posted on May 25, 2006 at 18:39hi, I use the communication between ST72F321 and memorie EEPROM 24c65 of microchip. all alone program I2C functions well in Reading & writing in the memory. but when I use interrupt Real Time Clock (RTC) [ MCCSR eo Tim...
Posted on February 15, 2006 at 19:18yes i read it, but i'm in simulation stade. so we can't simulate VPP at 12V. it'is necessairy for simulation !!? thanks
Posted on February 15, 2006 at 07:42hello, i want to simulate a emulated data eeprom in STVD7 3.1.1. so when i looking in the memory area, i view a data stored in the flash memory and i found : $FF it's mean that no change in the memory case. somebo...