Posted on October 29, 2008 at 18:59Dear All, I'm devepoling an application using an STR711FR2 and EMBOS Operating System with Keil uVision3 IDE. In my application I have an interrupt coming from the RTC at 32Hz. The MCU have to do some operations th...
Posted on February 24, 2007 at 08:36The advantage il that the new word is put into the fifo anc your CPU has not to wait for the previous word to be transmitted. If you turn off the SPI FIFO and have a look to the signal with an oscilloscope you can...
Posted on February 13, 2007 at 18:57Hi all I'm trying to use the freeRTOS port for str710 with Realview compiler. I'm having several problems the main problem is how to include .s79 in the project: are the same of .s files? Thankyou for your help an...
Posted on December 14, 2006 at 07:59Hi we found a good idea, we stop the RTC by shorting it to GND, when we reset the execution stops at the RTC into routine ad we can flash it another time