Posted on May 17, 2011 at 12:10hi, i used Upsd3333dv i search code for using uart0 and uart1 with timer1, timer2 i use timer2 with uart1 it's ok I pass in the interrupt of the uart0 and i affect value in SBUF0 but octet are not send.
Posted on May 17, 2011 at 12:10hi, i used upsd3333dv timer0 -->1ms the uart1 at 9600bps using timer1 / 40MHz clk. when i activited Timer1 (ET1=1) timer0 is stop THANKS FOR YOUR HELP ///////////////////////////////////////////////////////////////////...