Posted on December 16, 2005 at 08:19Actually I did nothing with the project yet, just importing the gpio.h causes that problem. I came over that by changing the ''inline'' functions in the gpio.h into ''static inline''. It works now but am not sure ...
Posted on December 09, 2005 at 06:24Hello all I have a strange problem, I just included the ST library but I got a linker error as below. that happen with RCCU and GPIO with all the functions defined in the Header file of RCCU and GPIO. the error of...
Posted on November 29, 2005 at 07:41Hello ibtiss, iam using the GNU toolchain, i inculded all the files u mentioned, but i still need the makefile and the linker script, these two are really confusing me. iam new to that field would anyone please up...