Posted on October 26, 2009 at 05:31Hi, In several projects we use the ST10F269 controller. We would like to use the ST10F276 in future. However, the firmware has to be compatible to old PCB’s with the ST10F269. As it is easy on runtime to determin...
Posted on March 29, 2006 at 11:06Hello, We are already changing the PCBs. However, the problem is that we have several PCB's which have been operated for days with this error. So my question is: is it likely that the microcontrollers are damaged? If...
Posted on March 29, 2006 at 09:19Hello, I connected the DC1 and DC2 pins of the ST10F269 abusively to +5V and worked with that PCB for days (yes I know, it's very stupid, but the PCB was first designed for a C167CR). It worked without any problem (a...
Posted on December 22, 2005 at 09:48 Hello, I have a problem to set the FLASH read protection in the ST10F As it not possible to set the Flash read-out protection of the ST10F269 using the Flasher Tool, I build in a small program in the cod...
Posted on December 13, 2005 at 07:09Hello, My distributor told me that the same chip is used in the ST10F269Z1 and Z2, both having 256k FLASH. However, the upper 128k of the Z1 is not tested and so not guaranteed. Problem then is: I now have several...