Posted on March 05, 2007 at 03:46HI: Why my str7 USB only receive Set_RePort request, but can not receive Get_RePort request? in usb_prop.c, code like this: .... else if((Request_No == SET_REPORT)&&((Device_Info->USBbmRequestType &(REQUEST_TYPE...
Posted on January 09, 2007 at 22:21 I programe application data in Bank1 of Str710, and the write operation command is executed from Bank0. when it write data into it, system will be reset.If I execute these code in external memory, it's ok! why? so...
Posted on September 18, 2006 at 00:11I use STR7's USB as mess storage , and I use extern flash memory(MX29LV640BB-90) as the medium memory,some time I can copy file to this disk, but some time , the PC will show '' the path is too deep'' or ''the pa...
Posted on February 21, 2006 at 06:29hi, thanks! AS I write some error code into the onchip flash memory of the STR710, I can not set the EIC of this STR710 for ever,it all EIC register is zero. I remove it and replace a new chip,so everything is OK...