Posted on June 23, 2006 at 08:24Hi Moe, Did you resolve IAP with USB. If you have, do you have sample code that I could use for my project. What gui did you use on PC side ? Thanks, Mik
Posted on June 23, 2006 at 08:10Can someone help me resolve calls to a function table which can pass parameters, I am struggling with this. Mik ~~~~~~~~~~~~~~~ CODE ~~~~~~~~~~~~~~~~~ // Start of Test module typedef void (*fptr)(void); typedef unsign...
Posted on November 24, 2005 at 09:11Dear Forum, Has anyone implemented this on the STR710 or has any ideas. A tentative circuit from uP to the RJ45 and a sample code to implement TCP/IP would be useful. Thank you in advance and Kind Regards, mik