Posted on July 06, 2006 at 17:55I have a few questions regarding in application flash programming of the STR73x series. 1. Is there an str73x version of the IAP example that is provided for the STR71x (using using keil/ARM RVDK if possible)? 2. Does...
Posted on January 17, 2006 at 21:19In order to reduce power consumption, I want to use the nSTDBY pin to enable/disable the main oscillator. The idea is that the nSTDBY pin goes high (pull up) turning the main oscillator on. Assume that the micro is...