Posted on October 13, 2005 at 01:23Hi Hich, First i think it is a question without the answer 'yes' or 'no'.One MCU only can do something,not everything. just for power monitor system,our products will communction with the devices,such as power su...
Posted on October 12, 2005 at 10:25 thanks for Hich 's reply. i cared for st's arm just because it has four uarts and enough capacity flash to me,but with too little of sram,so maybe i don't think it as a good design. everybody can image a mcu wit...
Posted on October 10, 2005 at 12:08 there only 16K bytes sram with str730,but in fact it is too little to use it in the products,so i want to konw how to extend the sram without emi?