Posted on July 14, 2005 at 13:56Dear Alok, Thanks for your answer. I know that you can consider a NAND flash as an I/O device and that besides the multiplexed data/address bus there are some control signals like CLE and ALE. If however you need to c...
Posted on July 12, 2005 at 11:04Thanks for your answer. It is too bad that the search function does not work properly. After I had gone manually through all pages, I found that this item had brought up before in May 2004. There reference was made to...
Posted on July 11, 2005 at 08:00I am designing a board using the STR710FZ2 and want to use a flash memory connected to the EMI. Now there are several types of flash available. Do I have to use NOR flash or can I also use NAND flash on the EMI? Which...