Posted on October 11, 2005 at 15:17This problem may be related to one we are having with the SPI system, where if we try to read the Rx FIFO too fast we get bogus data. Try waiting 8-10 clocks (count to 4 in tight loop for example) between the FIFO ...
Posted on September 29, 2005 at 18:53We're using the STR710 to read data from an external ADC. The ADC acts as an SPI master and sends a 96 bit burst of data with an SPI clock of 500kHz. The data represents 6 16 bit values., and the burst frequency ...
Posted on July 05, 2005 at 17:10I have a question about the maximum current sink capability of the GPIO pins on the STR71x series. According to the datasheet, when a pin is assigned to push-pull output mode, it can source either 8mA (high current pi...
Posted on June 10, 2005 at 18:03I'm going to use the STR710 in an application where I don't need the EMI (just the extra 16 I/O pins). What do I do with the unused EMI pins? Can I ground them all, or leave them open? Best regards, Ben