Posted on May 26, 2009 at 05:52I think it isn't possible to execute code from the IFlash in BSL mode. For example have a look at the user manual of the ST10F272, chapter 15.2.4, ''Memory configuration in bootstrap loader mode'': ~~~~~~~~~~~~~ Moreov...
Posted on September 19, 2008 at 16:12Hi Stefan, at the first time you read out the messages from the message ram without set the bit TxRqst/NewDat to one in the command mask register --> the New Data bit remains set in the message object (and theref...
Posted on August 19, 2008 at 09:10Which value did you write to XSSCCON (with XSSCEN = 0)? Did you configure the XSSC for operating in master mode? How did you configure the XSSC - Pins (i think like described in Table 56 in the User Manual)?
Posted on October 08, 2007 at 12:36From the datasheet: ''At power on, and after Reset phase, if the presence of a 32 kHz oscillation on XTAL3 / XTAL4 pins is detected, then the RTC counter is driven by this low frequency reference clock: when Power ...