cancel
Showing results for 
Search instead for 
Did you mean: 

ST10F27x: fast external interrupts serve without set bit CCxIE?

mirco23
Associate II
Posted on September 19, 2007 at 13:15

ST10F27x: fast external interrupts serve without set bit CCxIE?

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
mirco23
Associate II
Posted on September 19, 2007 at 13:15

How must i understand the following statement in the UM0407, page 113:

''EXxIN inputs are normally sampled interrupt inputs. However, the interrupt handler circuitry uses them as level-sensitive inputs. An EXxIN (x = 7...0) Interrupt Enable bit (bit CCxIE in respective CCxIC register) needs not to be set to properly serve the interrupt request (or exiting from Power Down mode).''

Will the fast external interrupts always served as soon as IEN = 1 (regardless of the associated CCxIE bit)?