Posted on March 14, 2005 at 19:28Thanks for the code. I am having trouble building it, however. Message is: ''lcd.c'', line 189: Error: #20: identifier ''GPIO2'' is undefined GPIO_Config (GPIO2, 0x0004, GPIO_AF_PP); Yet all the include files appear...
Posted on March 14, 2005 at 12:53I see ''STR71x Demonstration Software for MB393 board'' but this is only object code and therefore of no help. However, I see that ''STR720 Demonstration Software'' contains abundant source code. Can this code be use...
Posted on March 14, 2005 at 12:17I am looking for source code that would allow to quickly try a few things on the Eval board. The only source code I found is the one that toggles the 4 LEDs attached to the GPIO port. Is this all there is? Where can ...