Posted on May 17, 2011 at 12:09Hi Everybody, I am using the two UARTs in my aplication. I manage to operate UART0 and partly of UART1, I can send data from UART0 to UART1 but I can't send from UART1 to UART0. I am using timer2 for the baud rate(for ...
Posted on May 17, 2011 at 12:09Hi All, I am working with uPSD3400 and I intend to work with the two UARTs. Is it possible to use one timer (TIMER2) for both of the UARTs? They are working with the same baud rate and not working at the same time. Tha...
Posted on May 17, 2011 at 12:09Hi All, I worked with uPSD3200 at the past and now I intend to work with the uPDS3400. I have old Keil uVision 7.0 with no upgrade possibility. Can I import uPSD3400 configuration to my old Keil version? If yes, How do...
Posted on May 17, 2011 at 10:18Hello ! Where can I find Drivers for the ST7MC to control a Brushless DC motor (the outputs of the controller are fed to a 3 half bridge) ?